FB#.SSITYPE

Description

FB#.SSITYPE sets the type of SSI device used for position feedbacks. The SSI protocol is flexible and compatible with different feedback models using different implementations. The protocols may differ in the data format of the serial position bits. They also may contain special configuration and flag bits.

FB#.SSITYPE is used when FB#.SELECT = 36 (SSI). It is ignored for other values of FB#.SELECT.

The following table lists the supported SSI types with protocol details and example manufacturers and models.

Value Protocol Models Notes
0 Binary position bits only Netzer DS-25-SF-S0  
1 Grey code position bits only Hengstler AD34/1217AF.0NSC0:5942  
2

1 status bit

Grey code position bits

3 flag bits

1 zero bit

Gurley VP12S08A2CN ‘Initializing move’ required before position values from FB#.P are valid and will cause position jump on completion. See encoder datasheet for details.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-06-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2
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
FB1.SSITYPE

3500h

12h

Unsigned8

-

-

Read/Write

No

FB2.SSITYPE

3501h

12h

Unsigned8

-

-

Read/Write

No

FB3.SSITYPE

3502h

12h

Unsigned8

-

-

Read/Write

No

FB4.SSITYPE

3503h

12h

Unsigned8

-

-

Read/Write

No

FB5.SSITYPE

3504h

12h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.SSITYPE

30560

7760

Unsigned8

Read/Write

-

FB2.SSITYPE

30561

7761

Unsigned8

Read/Write

-

FB3.SSITYPE

30562

7762

Unsigned8

Read/Write

-

FB4.SSITYPE

30563

7763

Unsigned8

Read/Write

-

FB5.SSITYPE

30564

7764

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SSITYPE

30560

Unsigned8

Read/Write

-

FB2.SSITYPE

30561

Unsigned8

Read/Write

-

FB3.SSITYPE

30562

Unsigned8

Read/Write

-

FB4.SSITYPE

30563

Unsigned8

Read/Write

-

FB5.SSITYPE

30564

Unsigned8

Read/Write

-